This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: logic level translator for I2C and I2S

Part Number: TXS0104E
Other Parts Discussed in Thread: TXB0104, TXS0102, SN74AXC4T774, SN74LVC125A

Hi Team,
We are using TXS0104E in one of our projects for level shifting a 3.3V I/O signal to 1.8V I/O logic.
My controller is a 3.3V I/O logic controller.
The end device is an audio amplifier.TLV320DAC3101IRHBT.
It has both I2S and I2C interfaces.
1). Is the IC TXS0104E, the good choice for my application.
2). Is there any 6 channel IC available for my purpose since we have 6 such signals from the TLV320DAC3101IRHBT to the MCU?.
3). I believe TXS0104E  is the best choice for I2C and I2S.
4). I believe I don't require any external pull-up resistors for I2C as they have integrated pull-up resistors to corresponding voltage levels.
5). I believe the IC TXS0108EPWR is an 8 channel variant of the IC TXS0104E, but it is not available in Mouser or Digikey.
6). Do I need to use TXB0104 for the push-pull application?. because this seems more suitable with mu application.