Other Parts Discussed in Thread: SN74LVC125A, SN74LVC126A,
Hi Team,
Customer is consulting whether we have slew rate requirements for received signal on 1OE and 2OE pins? Our D/S have not shown this spec.
Best,
Stanley
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Customer is consulting whether we have slew rate requirements for received signal on 1OE and 2OE pins? Our D/S have not shown this spec.
Best,
Stanley
All CMOS devices without Schmitt-trigger inputs have such a requirement. (And it's the same for the control and data inputs.)
If the datasheet does not specify it, look at other device in the same logic family. The SN74LVC125A datasheet specifies a limit of at most 8 ns/V; the SN74LVC126A datasheet has 10 ns/V.
So which one is for SN74LVC244A? Pls help us confirm it. The D/S of SN74LVC244A doesn't contain it. Thanks.
These limits are specified as maximum, so the most restrictive one is the smaller number.
But the D/S of SN74LVC244A doesn't have this info. If these limits are necessary, customer needs the confirmed info from BU side. Just simply tell me which one you recommend to customer. 8ns/V or smaller?
As far as I can see, 8 ns/V should work for any LVC device. But I am not a TI employee.
Hi Stanley,
Please use 8 ns/V as the maximum transition rate for this device.
Also note that this is always in the "Recommended Operating Conditions" section of the datasheet -- it is not a measured specification, but a recommendation for operating the device without any issues.
Operating a device with standard CMOS inputs using slow inputs can cause issues as described here: How does a slow or floating input affect a CMOS device?
Hi Emrys,
Customer just feedbacks other vendors like Nexperia 74LVC244APW, which has no slew rate requirements for 1OE and 2OE pins. So they want to double check with us that can1OE and 2OE pins be free of above 8ns/V transition rate requirements?
Best,
Stanley
That information is wrong; Nexperia's 74LVC244A has slew rate requirements on all inputs, including 1/OE and 2/OE.
The Nexperia datasheet says that "Schmitt-trigger action at all inputs makes the circuit tolerant of slower input rise and fall times". However, "slower" in this case means only up to the specified 10 ns/V, and not any slower than that. "Schmitt-trigger action" is not the same as real Schmitt-trigger inputs. The application note Understanding Schmitt Triggers says:
There are parts that have Schmitt trigger action. This means that they will have a small amount of hysteresis that will help with noise rejection but will still have an input rise and fall time limit. These will usually not have any VT specs in the datasheet and will have rise and fall time limitations specified for the inputs in the recommended operating conditions.
Please note that TI's LVC inputs also have Schmitt trigger action, but the TI datasheet does not mention it because the Δt/ΔV specification (if the datasheet does not forget to include it) is enough to characterize the inputs for the circuit designer.