This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternate Part recommendation

Please help me to get a better alternate for TXS0104EPWR

Currently, we are using the TXS0104EPWR (4-BIT) part in the design for converting voltage level from 1V8 to 3V3. this is used for MDIO and MDC pin of Ethernet PHY.

With this part, we are facing IO level mismatch between CPU pins and Level Translator pins.

Could you please suggest a 4-bit translator part that supports MDC and MDIO pin ( Open-drain).

VIH of level translator should be less than 1.35

VIL of level translator should be greater than 0.45