Hi team,
I'm using I2C from carrier board to add on board with buffer P82B715DR on add-on board. Further to this level translator LSF0108 is used to use I2C at 3.3V.
Please see below SDA waveform with above described system (i.e. Carrier <__> Buffer <__> Level Translator ) :

After observing the SDA line waveform , I disconnected LSF0108 from I2C line by removing series 0 ohms. So the system was like :
(i.e. Carrier <__> Buffer ) . Now SDA line waveform looks like -

Can you please suggest what is causing issue is SDA line waveform with LSF0108 connected.
Also ,why after disconnecting LSF0108 the wave forms got clear. Please suggest.
Thanks,
mANOJ