Part Number: LSF0101
Hello,
We are using 21 Level Shifters (LSF0101DRYR) for level shifting between 3.3V to 5V. The output voltage from the regulator(TPS73233DCQ) which is 3.3V output is providing 3.9V while we populate all the 21 level shifters but if we populate less than 6 Level Shifters the output of the regulator is 3.3V. Can anyone suggest any solutions?