This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
From the datasheet, I can see that VIH minimum is VCCI – 0.2v on A port and VCCI – 0.4v on B port.
This means that if we have configured the device in such way that VCCA is 1.8v and VCCB is 3.3v and the data direction is B to A, is that mean that VIHmin = 3.3 – 0.4 = 2.9v? This means the the voltage swing must be very close to the supply voltages.
Am I understanding the datasheet correctly?
Jacob
I also forgot to ask if we have a SPICE model for the TXS0102.
The I/Os are not buffered. For signal voltages below VCCA, the TXS behaves as an analog switch, i.e., the A and B pins are connected directly. (For voltages above VCCA, the switch is open, and the pull-up resistor determines the output voltage.)
All signals have pull-up resistors and do not allow pull-down resistors, so they will go to the supply voltages.
Hey Jacob,
Here is an FAQ that covers this topic. Unfortunately, we do not have a SPICE model for this device.