This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVTH16244A: VOH(min) @Vcc=3.3V and IOL=-32mA

Part Number: SN74LVTH16244A

Hello,

My customer would like to know the minimum VOH when Vcc=3.3V and IOL-32mA.
According to the datasheet it is 2V when Vcc=3.0V and IOL-32mA.
So, you can just say it should be 2.3V (2V + (3.3V-3.0V)) when Vcc=3.3V and IOL-32mA?

Best regards,

K.Hirano