Part Number: SN74AVC16T245
Other Parts Discussed in Thread: SN74LVC2T45
The VIH of connected device has few margin when I use VCC=3.0V condition, so i would like to check if VOH could be increased when VCC=3.3V is used.
Could you tell me what the VOH min is when VCC=3.3V?
Also I consider VCC=5V. Could you tell me if the device will work properly with 1.8V input when VCC=5V is used?