AD1 is the output of 373, and the input is normal. There is no downward or upward peak. Where the red and rose red boxes are circled, please help to see what the problem may be?
1. I try to connect a 100 Ω resistor in series with the AD1 output pin of 373;
2. I try to connect a 0.1uF capacitor to GND in parallel at the AD1 output pin of 373;
Are the above two methods helpful? Is there any other proposal?