This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have refer datasheet of both the part mentioned in subject, from datasheet of CD74HCT240M I understand that each output can sink and source 25mA however same information(per output sink and source capability) I am not able to obtain for SN74HCT240D from datasheet.
My design requires sourcing 18mA current from each output pin. Requesting some information from community member
Regards,
Niral
Hi Clemens,
Thank you very much for your answer.
Can the part number you suggested provide 18mA without voltage drop from every output at a time?
All outputs have a voltage drop. But that of AC outputs is smaller; see the VOL/VOH specifications. Also see [FAQ] What is the output voltage (VOH or VOL) when the output current is X or the supply voltage is Y?
What is your actual application? Do you need separate outputs, or 144 mA total? At what voltage?
Application is 8x8 dotmatrix driver. Each Output is connected to anode of 8 column of LED in dotmatrix array so output must source 18mA to LED.
Currently I have used 74HCT240D but not getting enough brightness even if I use 20OHM resistor and I have found that voltage is getting dropped same as you mentions in earlier post.
Then the ACT240 is a good solution. If the input signals are not TTL, you can use the SN74AC240 instead. For a non-inverting buffer, use the SN74AC244/SN74ACT244.