This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Backlight driver

Hi,

I am using a LED Driver ADP8140ACPZ-2-R7 to control the brightness of the Backlight LED Module which is having the following specifications.

DAY MODE = 28.5V+/- 0.5V @ 50-60mA

Nightmode = 26.5+/- 0.5V @ 5mA

Backlight Driver Settings:

Mode = PWM

Current setting = 60mA max

Weeks back it was working fine and i was able to control brightness by varying Duty cycle of 1% to 99.9%.

Now, I am facing an issue with brightness control of LED Module.

Vreg = 3V

EN = High

@ 100% DC and 28.7V, 60mA drawn by Driver and Brightness is present(Not very high).

@ 1% DC,28.7V, 59mA drawn by Driver and Brightness is present( no change).

1. Even though PWM is changing from 99.9% to 1%, Why is current drawn by driver not changing?

2. Do i need to change any settings?

Request your feedback to resolve the issue.

Thanks and Regards,

Pedaiah G


Backlight driver.pdf