Part Number: LSF0102-Q1
There is a recommendation to use 300Kohm between VREFB and 5V,why is this needed?
Our application is 5V to 3.3V translation,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0102-Q1
There is a recommendation to use 300Kohm between VREFB and 5V,why is this needed?
Our application is 5V to 3.3V translation,

This resistor is needed to limit the current that flows into Vref_B and out of Vref_A, and to drop the voltage at the EN pin to VGS(th) above Vref_A.
Hi Clemens,
What will be the impact of not having it? . Customer has missed provision in PCB !.
Regards
Dilip
A-side output signals will not be clamped tp 3.3 V.
The current flowing out of Vref_A and into the 3.3 V supply is not limited. If the supply cannot sink this current, its voltage might rise, and damage any devices connected to it.