Hi Expert
My customer use case as below:
pin1 always =5V(Pin1 connect to VCC)
Pin 2 normally is float and triggered low voltage when system fault.
Y connect 3.3V voltage that normally current is limit 100mA.
when Pin2 tie to low, Y will sink current and output low

question:
when they doesn't set the 3.3V output current limit and pin2 tie to low, the output voltage will keep 3.3V and the sink current is 180mA. customer want to know: why device can sink 180mA, which part need this huge current in internal of device?