Part Number: TXB0102
Other Parts Discussed in Thread: TXU0102, SN74LXC2T45
Hi there. I'm looking for a level shifter/buffer for an SPI master running at 1.8V to 8 slaves at 3.3V. And in a package rated for 125C. Individual OE control by the Master. MISO will not be used.
I'm a little unclear on which product line to use between TXB0102, TXU0102, SN74LXC2T45, etc. They seem very similar to me. The TXB0102 has a buffered architecture but I thought all of these are acting as a buffer. What exactly does that mean. It looks like the SN74LXC2T45 might be best suited but I'd like to understand the differences better. Thanks for any help!