This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774: output to output skew

Part Number: SN74AXC4T774


We plan to use SN74AXC4T774 for translation from 3.3V to 0.75V.

From the datasheet, Tpd is 10ns max.

What is the maximum skew between two different outputs of the same device?

(What is the Tpd tolerance between two outputs)

Assume that PCB traces and load are identical for the two outputs.