This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: IO levels for LSF0108PWR translator

Part Number: LSF0108

I have gone through the Datasheet of LSF0108PWR part to get minimum and maximum voltage levels of VIH, VIL, VOH and VOL but unable to find clear information.

This is required to verify the interfaces between MCU and translator IO.

MCU is working on 1.0V logic level which needs to convert 3.3V using this level translator. Similarly, 3.3V logic level needs to convert 1.0V to interface with MCU.

Please provide above requested information by considering VREF_A=1.0V and VREF_B=3.3V.