This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Outputs from the SN74HCS125-Q1 will be going off board through a 2m, 100-ohm cable. I cannot add anything on the receiving board which has a LMX2595 receiving the signals.
Question: do I need to add a driver to the outputs of the SN74HCS125-Q1 to ensure a good signal on receiving end, or will the buffer allow enough drive? If any driver is needed, any suggestions which would work best?
Thank you for your suggestions
A strong driver would require termination at the receiver.
Your only choice to avoid reflections at the unterminated end is to add source termination. The typical HCS output impedance is about 30 Ω, so add a series resistor of about 70 Ω. The total capacitance of the cable and connectors, together with that 100 Ω, forms a low-pass filter and will limit the maximum data rate you can achieve.
Thank you. I am able to add source termination on the receiving end. What would recommend as a driver on the source?
That is exactly the information I was looking for. So, I will use the SN74LVC125A-Q1 as the driver, and add the resistor + cap. What is the advantage of using the AC configuration vs Shunt?
Hi Derek,
Shunt
" There are several disadvantages to shunt termination. Usually the line impedance is fairly low (50 Ω to 70 Ω), which requires a resistor of similar value. This causes a heavy dc current drain on the source when in the logic high state and requires a strong line driver to source the current. With the low-impedance resistor pulling to GND, the VOH of the transmission line is lower, reducing the noise immunity at the receiver. Additionally, having a strong pull down on the transmission line might unbalance the rising and falling edges of the signal, causing the falling edge to be faster than the rising edge, resulting in duty-cycle distortion of the signal"
AC
"AC termination (see Figure 13) has the precise termination advantages of shunt termination, but reduces the disadvantages of dc current drain and waveform distortion. At each transition of the signal, the capacitor charges up to the voltage level necessary to maintain zero volts across the resistor. During the arrival of the next input transition, the signal drives the full value of the resistor until the capacitor can again recharge."
This is from that same app note that Clemens posted.
Regards,
Owen