Other Parts Discussed in Thread: TCA9800,
Hello all,
Could you please suggest an I2C level translator which have Vil (Input Low) greater than 0.4V?
The source microcontroller I2C actually have VOL of 0.45V, that is the reason.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LSF and TXS voltage translators work like an analog switch; see [FAQ] Why are the TXS01xx VIH/VIL specifications so stringent?
Use a buffered translator like the TCA9800/1/2/3.
There is no buffered translator with the same pinout.
What is the test condition of that 0.45 V value? It is likely that the actual current is smaller, and that the actual VOL also is smaller. Furthermore, even if the LSF input voltage is higer, this will just increase the output voltage (see the FAQ linked above), which is usually not a problem for I²C devices.