Part Number: SN74LVC1G74
Other Parts Discussed in Thread: SN74LVC2G17, , SN74LVC1G08
Hi sir
Our design is a 19V DC in, so I use the BJT to transfer the voltage to 5V.
And this project need to use the tact switch as the power button,
so we try to use the SN74LVC1G74 and SN74LVC2G17 to implement this function.
And we need the thermal sensor(over temperature will pull down at OS/ALERT pin) to do the thermal cutoff,
so we add the SN74LVC1G08 to combine the signal from power button and the thermal sensor.
Could you help to review whether this design can workable?

Thanks.