This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please help me to pick up right inverter for crystal oscillator?
The input voltage is 3.3V. The oscillation frequency is 20-40MHz.
The load capacitance is ~10pF each.
Two output channels are needed.
From the app note below, I found the combination of unbuffered and Schmitt-trigger inverter is recommended for crystal oscillator application.
https://www.ti.com/lit/an/scea099/scea099.pdf
So, is SN74LVC2GU04 + SN74LVC2G14 good choice?
Best regards,
Itoh
These functions are combined in the SN74LVC1GX04.
When using two crystals, use two devices. If you need two outputs from the same clock, then a single LVC output should be strong enough, but if you really want two separate outputs, use a buffer like the SN74LVC2G34.
Hi Clemens-san,
Thank you so much for your suggestion!
By the way, I wonder why the app note doesn't list SN74LVC1GX04 as the recommended inverter.
I recommend you to update E2E Logic FAQ for oscillator, and SCEA099.
Regards,
Itoh
Hello Itoh-san,
I recommend you to update E2E Logic FAQ for oscillator, and SCEA099.
Thank you for the recommendation.
Can you direct me to the FAQ that you are referencing? Or do you mean that we should create one to answer this type of question?