Part Number: SN74GTL2003
Other Parts Discussed in Thread: TXU0104, SN74AXC8T245, , LSF0108
Hi
We are using this level translator on our board for SPI interface at 6MHz.
A-side(SREF) voltage is connected to 1.2V and B-side (DREF) voltage is connected to 1.8V. with this we are having an issue with the high-level voltages for signals on the B-side or only max up to 1V it is not reaching 1.8V why is this? and also the rising edges look so sloppy why is this happening? what is the fix for this?

Thanks
Santosh