Hi TI Team,
Currently, I have to face the overshoot/undershoot at the output of SN74LVC1G08
There are 2 situations when ringing appears:
1. The long trace is connected to the output. This is caused by mismatch impedance. I can simulate by using IBIS model
2. Short trace is connected to the output. I don't understand why ringing still appears in this case. And I use IBIS simulation but I don't see any abnormal signal
I see light load condition is also a reason why ringing happens. Is it explain why ringing in short trace ?
And in order to reduce ringing, I need to add a serial damping resistor. Is the damping serial resistor always needed?
Do you have any solution to save the cost and space than using damping resistor ?
Thanks,