This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC16T245: Channel to Channel Skew

Part Number: SN74AVC16T245
Other Parts Discussed in Thread: TVP5158,

We need to voltage translate the +3.3V output of the TI TVP5158 Video Decoder to +1.8V to match an FPGA I/O.  The 10 bit data is being clocked out of the TI TVP5158 at 108 MHz.

I would like to use the SN74AVC16T245 to translate the 10 data bits + clock. I have 4 questions

  1. The timing for VCCA = 1.8V, VCCB = 3.3V is tplh(min) = tphl(min) = 0.5ns   and  tplh(max) = tphl(max) = 7.4ns  ( B to A ).  But what is the channel to channel skew ?
  2. Is the channel to channel skew the same between the two groups of 8 ?  For example is the skew for 1B1 to 1A1 the same as between 2B1 and 2A1
  3. The datasheet states that the max data rates for 1.8V to 3.3V translation is 380 Mbps.  Is that for an individual channel ?
  4.  What is the Cpd(A) and Cpd(B) @108 MHz for our clock and 54 MHz for our data ?