This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G126: Operating with VCC of 1.05V (+/-0.05V)

Genius 17625 points
Part Number: SN74AUP1G126

Hi Team,

Can you please share your insights about SN74AUP1G126 operating with Vcc of 1.05(+/-0.05)Vcc:

I am actually concerned with the VIL and VIH of this device. With the given Vcc and its tolerance, since the VIL/VIH is dependent on the VCC, as per datasheet records and using interpolations (as guided HERE), I come up with the following:

So, there would be different VIH(min) and VIL(max).

Question:
Is it recommended to operate the device with such Vcc (including the 0.05V tolerance)?

Regards,
Archie A.