Part Number: LSF0102
Other Parts Discussed in Thread: LSF0108, , P82B96, TCA9803, TCA9617B, TXS0102, TCA9800, TCA9517, TCA9517-Q1, TCA9416
Hello,
I am designing a FMC board for the communication between two main boards. The FMC board will be connected to both master and slave boards and two FMC will be connected through Cat5 ethernet cable. Master is foreseen to control 2 different I2C pairs (SCL1-SDA1 , SCL2-SDA2). Because of the incompatible VOL problem of P82B96, I am forced to use lsf0102/lsf0104/lsf0108 for configurable voltage level translation between Master and Slave Boards. The distance between two boards will be around 10 meters. On datasheet, it is stated that LSF series can be used up to ' 40 MHz up or down translation at 50-pF capacitive load' . I would like to ask if the maximum capacitive load value changes with lower clock rates like 100kHz I2C. If yes, can you please provide information about the foreseen value so that I can try to figure out maximum distance I can transmit my signals through Cat5 ethernet cables. I am aware that 10 meters is far away. Depending on the maximum distance achieved with LSF series, I am planning to design an intermediate repeater board between two FMC.

Selim