Other Parts Discussed in Thread: TXU0104, TXU0204,
One of our circuits uses the level conversion chip of your company TXB0108DQSR. The load device is the scanner dock (3.3V), and the control signal is output by the CPU (1.8v). The current phenomena are as follows:
1, when connected to the scanner dock, the CPU will not pull up, and the waveform is a high level with concussion. Remove the scanner dock, the high level can be pulled up normally;
2, if the oscilloscope point at the load end can be normal output high level, if you do not use the oscilloscope probe point here, it is not working normally.
3, replace Onsemi's level conversion chip(NLSX3018MUTAG) can normally output high levels.