I have a simple question. Positive impulses with the duration 10 microseconds and the amplitude about 5 volts comes from out "Q" of the CD14538B (monostable multivibrator) to the pin number 5 "C" (one NAND-Schmitt) of the CD4093. Between pin number 5 "C" and pin number 6 "D" included the resistor 10 kOhm and fast impulse (Schottky) diode - its cathode connected to the pin 5 "C"of the NAND-Schmitt and its anode respectively connected to the pin 6 "D" of the NAND-Schmitt. Also, pin number 6 "D" connects with the ground wire via the capacitor 150 pF. So the inverted negative impulses gathering from the pin 4 (out "K") of the CD4093. What was the purpose of connecting the resistor and the diode between pins number 5 and number 6, and for what the capacitor 150 pF was connected with the pin number 6 of the NAND-Schmitt and the ground wire? Wouldn't it have been easier tied together pins 5 and 6 and connected them with the out "Q" of the CD14538B? In another (old) version of the circuit it was done as I described. How does this affect the waveform at the inverter output ( pin 4 out "K") of the CD4093? Maybe it reduces the noise level? Or is the impulse-shaping depends on it? Could someone explain it for an old student?) Above described part of the circuit was used in the analog survey meter. Thanks!


Hi Ian and Emrys! Thank you both for your responses. The circuit I've described is the small part of the Bicron Micro-R Survey meter scheme it`s a micro-Rentgen counter.