Part Number: TXB0108
Other Parts Discussed in Thread: LSF0108, , SN74AXC1T45, SN74AXC8T245, SN74AXC4T774, SN74AXC4T245
Hi team,
My customer mow is using NXP's NXB0108PW.
And now they have a test condition: 5 ns voltage pulse.
Could you please kindly help check below questions:
- If they want to transfer this 5ns pulse, is that means they need a device with the 200M data rate?
- I saw we have a figure in LSF0108: Figure 6-1. Signal Integrity (1.8 to 3.3 V Up Translation at 50 MHz), Could you please help check if we have the figure for 100MHz?
- Could you please help check if these 3 device can meet their requirements for 5ns pulse? Will there be any distortion?
- Could you please kindly help recommend a device for the 5ns pulse?
Thanks,
Brian