Other Parts Discussed in Thread: LSF0102
Dear,
I am a HW-engineer working at Innogrit. My name Hans Liang.
I have met some level translate(3.3V ~ 1.8V at SMBUS) issues at our enterprise-SSD drives with using TXS0102DQER and TXS0102QDCURQ1.
We found that maybe the one-shot feature cause the failure. Because the low voltage at host is about 0.6V and the VIL at TXS0102 is ≤0.15V. We guess that the 0.6v false triggering the one-shot, then the communication at SMBUS is fail.
Now, my question are below:
1/ Do you have the Pin to Pin samples without one-shot compatible with TXS0102DQER and TXS0102QDCURQ1?
2/ Do you have the Pin to Pin samples with higher VIL, such as 0.6V instead of 0.15V?
we need your emergency help. Our projects are being at a critical schedule.
Thanks very much!