Part Number: CD4504B
Other Parts Discussed in Thread: SN74LV6T17, OPA4197, TXH0137D-Q1
Hi Clemens
Thank you for your prompt answers as always.
While your answer was meticulous and rigorous and I thank you for that ,
if I were to reduce my Source & Sink requirements to 5 mA Max, which would be
adequate for my IGBT Drivers while accepting a Vds of 2.5 Volts @ Vdd of 15 V,
Vcc as 3.3 V and Mode Selected as TTL to CMOS , this IC looks reasonably okay
as per the Fig 11 on Pp 3-244
Can you please have a re-look ?
Can avoid having to use Two Packages as one from 3.3 V to say 5V , then using this IC to +15V
Best regards
Varun