This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102: Questions of LSF0102

Part Number: LSF0102
Other Parts Discussed in Thread: TXS0102

Dear Team,

Currently, there is a case where LSF0102DCTR is used and the signal high level of Port B does not reach the voltage of Vref_B (4.2V), only about 2.2~2.3V.
The Port B signal is connected to TLC59208FIPWR. Even after adjusting the resistance of R45 and R48 & R49 to a smaller value, the same problem remains. Can you please help confirm which side of this part is the problem? Thank you.

Many Thanks,

Jimmy