Part Number: TXB0104
Other Parts Discussed in Thread: TXU0304, TXU0202
Hello.
I want to use TXB0104 AS SPI BUS LEVEL SHIFTING/TRANSLATOR 5V TO 3.3V.
I also will need RX TX (UART COMMUNICATION) TRANSLATOR 5V TO 3.3V IN THE SAME PCB.
I want to use 2 parts in my pcb.
My spi bus has low frequency speed 30Khz.
RX TX has 115200kbps and also RX HAS 10K Pull up.
Can i use TXB0104 AS LEVEL SHIFTER/TRANSLATOR 5v -3.3v for spi bus (low frequency 30Khz) and RX TX ( 115200kbps uart)?
Regards
Alex