Other Parts Discussed in Thread: TXU0304
Are there any issues with connecting the output (for example, A4Y) of TXU0304-Q1 together?
In the design that I am looking at, there are two SPI devices that we want to interface to one MCU. MISO from each SPI device would be connected to B4 of one TXU0304. Only one of the SPI devices would be driving MISO/B4 at one time. So you have a situation where "device 1" might have MISO/B4 high, "device 2" would have MISO/B4 low. Are there any issues at A4Y? Attempting to draw it...

Thanks!