This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Customer measurement found that U22 PIN8 has an abnormal waveform when USB is abnormal (USB_OC#_abnormal.png) U22 uses TXB0304RUTR
Changing RA43 to a smaller size (1K for testing) can solve this problem
May I ask how much should be changed to RA43 and RA44? Is there any reference material?
The TXB must not be used with strong pull-up/-down resistors (< 20 kΩ); see section 8.4.2 of the datasheet.
For unidirectional signals, you should use a unidirectional translator like the TXU0102. Are the directions of the two GPIO signals fixed?