This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXCH1T45: 50MHz issue: Translation from 3.3V to 0.75V

Part Number: SN74AXCH1T45

Hi,

We are using  SN74AXCH1T45DCKR in our design to convert 50MHZ and 100MHz clock signals from 3.3V to 0.75V level. 

We we tested this section on the board, we see that the signal towards 0.75V side is around 200mV level and has 0.75V DC level. 

We have to change the voltage from 0.75V to 1.2V to see proper 50MHZ clock ont he lower voltage side. But this is not an option for us. 

Request your support to suggest us solution to mitigate this issue.

Regards

Sharath Chandra