This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
With SN74LV1G74 this film, the input is 100M CLK, and the original reference project is to output a 50M differential clock, but now there are 2 problems
First, the output differential mode, I understand that it should be Q to CLK_P, nQ to CLK_N
Second, I see that this film also has a single-ended connection, if SN74LV1G74 use single-ended output, what is the output CLK frequency? My current demand is to output a single-ended 50MHz CLK, but I don't see any configuration
For the differential clock, you are correct. /Q will be the "positive" clock and Q will be the "negative" clock.
For the single ended output, the effect is the same. The output frequency should still be 50M.
Please let me know if I am misunderstanding the question.
Best,
Malcolm