This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G123: DEMODULATOR CIRCUIT FOR IR SIGNAL

Part Number: SN74LVC1G123


We have used IC [MPN:- SN74LVC1G123YZP] for demodulation of IR signal so

1. please review this circuit and provide confirmation that it is right part for this application
2. and also share you feedback on review the circuit.



Check below example waveform of
Waveform 1 --> Signal name=IR_SIGNAL_IN [Modulated IR signal coming from IR Receiver sensor] &
waveform 2 --> Signal name=IR _Signal [Output of the SN74LVC1G123YZP IC [Pin-5] which is Demodulated IR signal ] 
IR Receiver Part:- TSMP1138 [PFA datasheet]

TSMP1138-Vishay.pdf