Other Parts Discussed in Thread: CD74HCT4538
Tool/software:
I am currently working on a high-reliability design project that involves using the SN74LVC1G123 and the CD74HCT4538E components.
Question#1:
Could you please verify that it is strongly recommended to add a 51 Ohm resistor in series with Cext when the capacitance is above 0.1uF when using the N74LVC1G123 and CD74HCT4538E ? What other ideas or recommendations do TI suggest?
The Cext capacitor is located between (Rex/Cext and Cext) and is connected in parallel to the internal drain and source MOSFET of either the SN74LVCG123 or the CD74HCT4538E. This enables the Cext capacitor to be discharged immediately when necessary. The resistor connected in series with Cext will help control the flow of current as Cext discharges.
Question #2:
Could you please refer me to a TI application note that recommends using a resistor in series with Cext for an IC where Cext discharges through a MOSFET and the Cext capacitance is higher than 0.1uF?
Kind regards
Slim