Part Number: LSF0102
Other Parts Discussed in Thread: LSF0002, LSF0108, LSF0204
Hi, I am looking for a solution to do a I2C - FAST MODE (400 kHz) Level translation from 1.8V to 3.3V. I have previously used LSF0102, but I cannot use this anymore as on the 1.8V side of the design I have Pull ups of 10kOhms fixed by the Hardware. Please note The Level Translator needs to be fitted on a sub PCB which is connected to the Host PCB using a FPC (a max. of 10pF is expected). The interfacing is shown in the simplified schematic below. The Datasheet for LSF102 discusses Pull up values, which work out to be < 1k. This is not ideal pull up for I2C. Can you advise on this please? Thanks.