Tool/software:
TI experts,
My application using this device requires switching VCCA via a transistor to induce tristate condition.
The specification SCES515M states: The VCC isolation feature is designed so that if either VCC input is at GND, then both ports are in the high-impedance state. Please expand on "...either VCC input is at GND"
Is this a high impedance state (ie. VCC is disconnected) or is there an impedance required to GND eg. a pulldown resistor or is there a minimum current into VCC. I see mention of Ioz in the Electrical Characteristics which appears to be the leakage current in tristate condition but no further mention of VCC conditions for tristate. Or have I missed something.
FrankCA