This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0101: TXS0101 - IBIS model Issue

Part Number: TXS0101
Other Parts Discussed in Thread: TXS0102

Tool/software:

Hi,

I am using an IBIS model of TXS0101 (instead of TXS0104(IBIS NA)) which has only input pin option to be configured.

I need to configure as an I/O from Vcc 1.8V to 3.3V and vice versa for an SPI application @10Mbps.

Kindly do confirm the behavior of TXS0101 and TXS0104.

Also provide me with an updated IBIS model ASAP.

Thanks and regards,
Sathish Raja C