This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello
We have such a issue. LDAC signals have a lot of clutter signals during each cold boot from -5℃ before FPGA loading complete . It will cause the DAC work abnormal.
LDAC is always high at room temperature. the issue can't be reproduce at room temperature.
Our design block is like this:
Here is our circuit:
The pull up resistor of LDAC_B is not populated at BOM.
If we populate the pull up resistor of LDAC_B, issue can't be reproduce at -5℃.
Here are abnormal waveform:
Can you help to explain why this issue happens at low temperatures and not at room or high temperatures?
Where exactly did you measure this waveform, on the FPGA side, or on the DAC side?
I measured at DAC side. The buffer input cannot be connected to an oscilloscope, otherwise it will affect the buffer output. The oscilloscope access terminal has a resistance and capacitance to ground, which is equivalent to a weak pull-down. If we connect buffer input to oscilloscope, the issue can't be reproduce anymore.
The problem is that the buffer's inputs are floating. This is forbidden; see footnote (3) in section 5.3.
You must add the pull-up resistors. (If you care about power usage, use a higher value, up to 100 kΩ.)
Thank you.I just want to know why this issue happened at low temperature, not at room or high temperatures
Apparently, at low temperatures, the leakage currents of your board keep the inputs near the switching threshold.