This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The device specification does not have a power supply tolerance specification. There is a table that suggests a tolerance "Pg 13" but it does not directly apply to a more general power supply tolerance specification.
Can someone define a tolerance for each power supply voltage the device is expected to operate at? If you need specifics, please supply tolerances for 1.2V and 3.3V power supplies.
Hi Thomas,
The device is recommended for a min of 1.2 V and a maximum of 3.6 V. Hence no concerns and can tolerate 1.2 V and 3.3 V power supplies, thanks.
Best Regards,
Michael.
This does not answer the question of power supply tolerance.
If one side is accepting 1.2V logic, it should have a 1.2V power supply for that side.
How much positive and negative variation can be tolerated before the device fails to recognize a valid 1.2V logic input signal?
1.2VDC +-??
The same applies to all valid logic level power supplies. What is the tolerance?
Hi Thomas,
Thanks for clarifying. Unfortunately, devices with 1.2 V as the minimum guarantees electrical characteristics for 1.2 V without negative tolerances and anything less is not guaranteed i.e. 1.199 V is not guaranteed. If lower voltage level is needed, see SN74AXC2T45, thanks.
Best Regards,
Michael.