Other Parts Discussed in Thread: TPS54418, SN74LVC1G126, SN74LVC2G126
Good Afternoon Team,
I am looking for a tri-state buffer for my SYNC CLK on the TPS54418. I want to be able to remove the clock input with high Z output on the buffer. I tried the SN74LVC1G126 but, it seems that that even with the buffer disabled (high Z output) the input clock has an effect on the output, see the plot below. This effect seems to be causing my SW node of my TPS54418 to change frequency slightly but rapidly.
Is there another part that will not allow the input clock to effect my output of my buffer, once the device is in high impedance?

yellow = buffer output, red = buffer input, SN74LVC1G126 disabled (high Z).
Condictions: 5Vcc, 0V - 4V square wave clk, 700kHz, output disabled.
This is what I am trying to do.

Thanks,
Michael Green