Part Number: TXS0108E
Other Parts Discussed in Thread: LSF0102, SN74LVC244A
Tool/software:
Hi Team,
There is GPIO, SPI and UART Interface between IC1 and CPU.
Following are the IC1 IO Levels (Type I and II).
VOHmin=3V, VOHmax=3.3V
VOL max=0.4V
VIHmin=3V , VIHmax=3.3V
VIL max=0.6V
It is interfaced to CPU with IO levels as follows.
VOHmin= 2.64V, VOHmax=3.3V
VOL max=0.66V
VIHmin=2.31V, VIHmax=3.3V
VIL max=0.99V
CPU to IC1 interface:
VOH>VIH is not met
VOL<VIL is not met
IC1 to CPU Interface:
VOH>VIH is met
VOL<VIL is met
Both devices operate at 3.3V supply.
TXS0108EPWR level translator if used between both devices, still specs fail.
VOHmin= 2.211V
VIHmin=2.9V
VILmax=0.15V
VOLmax=0.55V
what about LSF0102?
Kindly suggest.
Thanks,
Vidhya