This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC16T245: Can we use SN74LVC16T245 for VCCA=VCCB & Need to Follow any Power Sequence?

Part Number: SN74LVC16T245


Tool/software:

Hi,

Iam using (SN74LVC16T245) Part for Level Translation Application, In my case VCCB is Fixed & that IO Signals are 3.3V , VCCA Port Signals Can be 1.8V or 2.5V or 3.3V or 5V but Present it will be 3.3V IO Signals.

So in the above Mentioned Requirement it Clearly Says that at one situation it will be VCCA=VCCB, in datasheet it mentioned both VCCA and VCCB can be supplied at any voltage from 1.65 V to 5.5 V.  Now as per datasheet information will it work at VCCA=VCCB? &

Need to Follow any Power Sequence for Port-A & Port-B with available Combinations?

Thanks & Regards,

Akshai.