This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T774: cascade SN74AVC4T774 for SPI application

Part Number: SN74AVC4T774


Tool/software:

Hi Sir,

SPI clock rate around 5MHz

Do you recommend SN74AVC4T774 for the SPI application below?

What should we pay attention to in the application? for example, load capacitance

Do you have any requirements on the input signal of the level shifter? for example, rise time, fall time, etc. 

Thanks

Hector