This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Sir,
SPI clock rate around 5MHz
Do you recommend SN74AVC4T774 for the SPI application below?
What should we pay attention to in the application? for example, load capacitance
Do you have any requirements on the input signal of the level shifter? for example, rise time, fall time, etc.
Thanks
Hector
Hello Hector,
Yes, I would recommend the AVC4T774 for SPI applications. Since it is SPI, I would pay attention to the distance between the master and slave since this will increase your propagation delay. 5MHz is typical for SPI but if you happen to have a long trace/cable length, you may experience missing bits.
For input requirements, I would follow the recommended conditions found in the datasheet.
Regards,
Josh
Hi Josh,
Do you have examples showing missing bits when using long trace/cable length?
We will use a 130mm coaxial cable to connect main board and sensor board.
Thanks.
Hector
Hello Hector,
This reference design (TIDUED8) notes talks somewhat about the effects of prop delay on SPI clock and how LVDS could be used to resolve it. However, this mainly applies to cable lengths >1m.
I don't see an issue with using a 130mm coaxial cable to connect main and sensor board.
Regards,
Josh
Hi Josh,
Update the topology and list the number of slaves connected to the bus.
Do you have any concerns?
Thanks
Hector
Hello Hector,
I don't see any issues with the updated topology. Thanks.
Regards,
Josh