This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Can you please explain what is mentioned in the datasheet P19, which states it can be either OD or push-pull? Could you clarify this? The driving capability of OD is determined by 10K/VCC, but how can it also be push-pull? Thank you
Jeff
Hi Jeff,
The TXS is an open-drain based translator with internal 10kohm pullups, and is capable of supporting both push-pull and open drain driver architectures. Its intended design is to be compatible with auto-bidirectional signals therefore the driving capability is limited. If the intended application is to provide level shift and driving capability for push-pull signals, the TXU0x04 is better suited for this use case.
Regards,
Jack