This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
I am using this level translator for MDC/MDIO , reset, interrupt connections.
Pull up to be placed on either sides (pins 3,4,5,6?)
Pull up value can be 4.7K ?
Thanks and Regards,
Vidhya
Hi Vidhya,
Pullups are recommended on both the inputs and outputs of IC42. For IC76, pullups are needed on B2, but optional on A1/A2/B1 if both RESET and INT signals are push-pull driver based.
The value of the pullups are selected based on the desired speed on the signals. For estimation, this equation can be used:
Regards,
Jack
Regards,
Jack
Hi Vidhya,
Also, same pullup value is to be used on either side as it is a PASS device?
This is not a firm design requirement for the device, though note that during a logic LOW, the pullups on the I/Os will become parallel.
Regards,
Jack